Ubuntu’s unattended-upgrades commands and package features may not work as expected when using an Exacq Ubuntu image on ExacqVision hardware. By default on Ubuntu Exacq images, unattended-upgrades package features are purposely disabled from running due to the potential of losing video.
Tag: Patches
ExacqVision stance on Operating System updates
The official stance of ExacqVision regarding security updates and auto-updates is they are off by default, because there is the potential risk of the NVR being rebooted during the update process which can stop video recording, so please plan accordingly!!! ExacqVision cannot control the integrity of security patches or operating systems updates; therefore these off… Continue reading ExacqVision stance on Operating System updates