Exacq Client Username/Password Reset

*** INTERNAL USE *** If you are unable to login to the ExacqVision software and need to reset the password, perform the following: WARNING: This will remove ALL user accounts from the configuration, not just the admin locked out. Windows OS 1. Visit the following page and download the server version you need.https://www.exacq.com/reseller/legacy/?file=Legacy/index.html2. On a… Continue reading Exacq Client Username/Password Reset

Enterprise System Manager Shell

To open Enterprise Manager Shell in Windows, run Command Prompt as an administrator and change directories to the installation directory by running the following command: cd C:\Program Files\exacqvision\enterprisemanager \enterprisesystemmanager\ Then type: enterprisesystemmanager.exe shell To open Enterprise Manager Shell in Linux, open a Terminal window and type: sudo /usr/local/exacq/esm/enterprisesystemmanager shell <br> The following commands can be used… Continue reading Enterprise System Manager Shell