H.264 and H.265 H.264 (MPEG-4 AVC) and H.265 (MPEG-4 HEVC) are MPEG video standards. H.265 is the newer of these standards.<br><br> What is Motion JPEG? Motion JPEG is a compression format that is older than H.264/H.265 and was created as a version of the still image JPEG format for video use. It is often shortened… Continue reading What is H.264 / H.265?
Tag: P-Frame
H264 / H265 vs JPEG
What are the differences between H.264/H.265 and JPEG? Why would you choose to use one over the other? Learn the answers to these questions in the video above.