Categories
Knowledge Support Support Categories Products exacqVision Hardware

SCN-00000018 – OS-on-RAID

SCN #SCN-00000018
Title of SCNOS-on-RAID
TRAC #
Effective VersionLaunch scheduled for July 20th, 2020
Products AffectedA-Series  –  Z-Series  –  S-Series  –  EM-Series
Reason for Change (Summary)New Option

Change

The standard option for these machines will remain with a single SSD for the Operating System.  However, there will now be an option to add a redundant Operating System disk.  These will be attached to a physical RAID card in RAID 1 configuration.

This option will be available for all Z-Series, S-Series and EM-Series.  However, the A-Series will only have the option on the 4U (R4A) and the Front accessible 2U (F2A).  There is a significant cost difference for the A-Series option as the RAID card must be added.

Additional Documentation

The Hardware tab will now show both RAID volumes in the Tree or Graphic format.

The 4U Z-Series will have a bracket which holds both SSD drives.

The 2U Z-Series has a similar bracket.

The 4U A-series bracket is mounted underneath the drive cage.

Other information

For the 4U A-Series, one of the drive cages will need to be removed in order to replace the SSD drive.

If the system has a hot spare disk, the spare will take the place of the OS drive and will not be available as a spare for the data drives until the faulty SSD is replaced.

The RAID card can host both volumes, so only one card will be needed even for the Z-Series.  Both volumes will show as follows: