Operating System Release Notes

Systems built by Exacq utilize customized OS images for Windows and Ubuntu (Linux). There may be instances where it is necessary to check the release version on an Exacq system. The release notes are contained within the operating system in a text file titled Release_Notes located on the root of the OS drive. File path… Continue reading Operating System Release Notes

Can my NVR be Updated to Windows 10

Title Can my NVR be Updated to Windows 10   Description  For customers that would like to migrate from their current operating system to Windows 10, we offer a purchasable upgrade kit.  However you should first determine if the system is compatible / eligible for the upgrade.   Product  exacqVision ServerUbuntu Windows 7 Windows Embedded 7 (WES7) Solution… Continue reading Can my NVR be Updated to Windows 10

Updating Windows Operating System

Windows To update your Windows 10 Operating System: Open Windows Update by right clicking the Start button in the lower-left corner and select search. In the search box, type Update, and then, in the list of results, click either Windows Update or Check for updatesClick the Check for updates button and then wait while Windows looks for the latest updates for your computerIf you… Continue reading Updating Windows Operating System

Update Ubuntu Linux Software Using Command Line

Installing updates via Terminal The commands are as follows: apt update: Update is used to resynchronize the package index files from their sources on Ubuntu Linux via the Internet.apt upgrade: Upgrade is used to install the newest versions of all packages currently installed on the Ubuntu system. To update software list for Ubuntu First, open… Continue reading Update Ubuntu Linux Software Using Command Line

ExacqVision stance on Operating System updates

The official stance of ExacqVision regarding security updates and auto-updates is they are off by default, because there is the potential risk of the NVR being rebooted during the update process which can stop video recording, so please plan accordingly!!! ExacqVision cannot control the integrity of security patches or operating systems updates; therefore these off… Continue reading ExacqVision stance on Operating System updates

LC Client or Operating System freezing

Description  LC’s with the ASRock H110M-ITX motherboard may show the video images freezing, followed by a freeze of the Operating System. Workaround 1 Set VGA acceleration to noneNote that this also means GPU decoding is disabled Workaround 2 Install 9.4 or higher clientInstall libegl1-mesasudo apt-get install libegl1-mesaThis should already be included on systems with the… Continue reading LC Client or Operating System freezing

Changing the OS admin password on exacqVision Linux machines

The process to change the admin password for the Operating System varies depending on which version you are using. The OS version can be found by entering the following command in a Terminal: cat /etc/issue Use the Contents menu to the left to go directly to the version of your operating system. <br> Ubuntu 18.04… Continue reading Changing the OS admin password on exacqVision Linux machines

Should I upgrade the operating system of my exacqVision recorder to the next major version?

Should I upgrade the operating system of my exacqVision recorder to the next major version? Operating system vendors periodically release new major versions of their operating systems. A major version upgrade is generally identified as the first number of the version increasing (E.g. Ubuntu 10.04 to 12.04), or the name of OS changing (E.g. Windows… Continue reading Should I upgrade the operating system of my exacqVision recorder to the next major version?

Does ExacqVision work with 64-bit Windows?

ExacqVision Server software has supported 64-bit Windows since Server version 6.4. sDVR and tDVR analog capture board installers for 64-bit Windows ExacqVision Hybrid systems are also available. For a list of currently supported operating systems, refer to the software product pages on Exacq.com, then click ‘System Requirements.’ <br>