Pelco plugin with Optera crashes server

Description Pelco plugin with Optera crashes server. ExacqRtsp_lib getSdpValue function is used by Pelco Optera to get the dewarp information with the RTSP session. The camera fails to return sdp and the default return of the getSdpValue method is NULL in this case. Line 1148 ExacqRTSPCommandHandler.cpp. <br> Tested Version <br> Steps to reproduce <br> Expected result Server… Continue reading Pelco plugin with Optera crashes server

Pelco Optera supports Panomersive Uni-stream mode

Description Pelco Optera is a multi-sensor 180/360 camera that provides panoramic views. We started supporting this model with r101894 dev build 7.9.32.101939 and officially in 8.0.0.102418 RC. <br> Fix The camera should be set to the “Panomersive Uni-stream” mode.In the camera web page, got to the “System” tab and under “Optera Compatibility Mode”. Let the camera reboot… Continue reading Pelco Optera supports Panomersive Uni-stream mode