In some installations users may want to allow users to automate the process of opening multiple client instances on different monitors of a workstation. This article details the steps to create an XDV file that will open the client to the configuration of your choice. Click the exacqVision logo in the top-right corner of the client… Continue reading Opening exacqVision Client on Separate Monitors Using Short Cuts with Client 9.4 and Higher
Tag: Opening Client
Opening exacqVision Client on Separate Monitors Using Short Cuts with Client 9.2 and Earlier
If you are using exacqVision Client 9.2 or earlier and want to create a shortcut that allows your users to open the client to a predesignated camera view, event monitoring profile, or to specific monitors on a multi-monitor viewing station, you will need to create an XML file based on the client CLI documentation: If… Continue reading Opening exacqVision Client on Separate Monitors Using Short Cuts with Client 9.2 and Earlier