Dewarper Workaround

Issue Both Axis and Pelco depend on OpenGL for dewarping.  If dewarping is not working for a Windows client because of GPU driver issues you can use the following open source Mesa3D software OpenGL drivers as a work around.  This will basically use a software implementation of OpenGL to do the dewarping which is really… Continue reading Dewarper Workaround

What is the VGA Acceleration Mode feature on the Client page?

The process of decompressing and displaying hundreds of video images per second is processor-intensive. It is possible to use the capabilities of modern display adapters to offload the main workstation processor from some of this work.<br> The ExacqVision Desktop Client tries to automatically determine the best operational mode and colorspace for the available display hardware.… Continue reading What is the VGA Acceleration Mode feature on the Client page?