Removing Unused LSI MegaRAID Storage Management Software on Ubuntu Linux to Eliminate Open Port 3071 Vulnerability

Vulnerability scans may detect and indicate that port 3071 is Open/Listening because of the installed LSI MegaRAID Storage Management software (LSI MSM) on an Ubuntu Linux server that does not have hardware support for RAID configuration. IF IT IS NOT BEING USED, the software may be removed to eliminate this vulnerability.