Description Motion will stop working on FLIR models after updating from exacq Server 24.09.5.0 to exacqServer 24.12.7.0. Product CAMERAS:Flir FC-317-IDFC-324-IDFC-332-ID Steps to Reproduce Update exacqServer to 24.12.7.0 motion events will stop working properly. Expected Results Motion should work. Actual Results Motion Stops working upon updates to 24.12.7.0. Solution Test build exacqVisionServer_24.12.2239205.0_x64 is working25H1 will house… Continue reading FLIR Camera Motion Stops Recording Motion Events
Tag: ONVIF Motion
Avigilon Camera Motion Detection Fails on exacqVision Server 24.12.7.0
Description When updating Exacq Server to 24.12.7.0 motion events will stop registering in the Camera Setting page under status last motion event. Motion Events are not being recorded. Product Steps to Reproduce Expected Results Actual Results Solution
AVCostar AV20576RS Stop Recording Motion Properly When Updated to 24.12.7.0
Description AV20576RS will show Motion recording in random recording states when updating Server to 24.12.7.0.In some Instances the cameras would allow some channels to recording while others stop seen below. Another issue seen was that motion would continuously record. Another Issue was observed where motion would just stop. Product Steps to Reproduce Update server to… Continue reading AVCostar AV20576RS Stop Recording Motion Properly When Updated to 24.12.7.0
Motion is not working for All ONVIF cameras on Exacq Server 24.06 & 24.09
Description Motion recording is not working on all ONVIF cameras with Exacq server version 24.06 & 24.09. Some analytics may not work on some brands. Product Exacq server versions 24.06 & 24.09 Steps to Reproduce Connecting ONVIF cameras or any supported brands via ONVIF to exacq server ver 24.06 or 24.09 and trying to trigger… Continue reading Motion is not working for All ONVIF cameras on Exacq Server 24.06 & 24.09
Pelco SMLE1-15V5-3h Motion Events are not Received by Exacq
Description The Pelco SMLE1-15V5-3h does will not record or see last motion events in exacq client/ server.Both Firmware’s were tested and work with the override.4.80.0.24(F722c136)and fw 4.86.0.20(7a7d6563) Product ExacqVision Server 24.03.7.0 – 24.09.4.0 Steps to Reproduce Set up motion in the cameras gui for each head in the camera to enable motion events. Expected Results … Continue reading Pelco SMLE1-15V5-3h Motion Events are not Received by Exacq
ONVIF Cameras May Stop Recording Motion
Issue Some ONVIF cameras report motion by means of a “pull-point” connection separate from the streaming video connection. If the camera unexpectedly closes the motion status connection, the server will retry the connection in order to reacquire motion status. When this happens, the corresponding server log messages will resemble:4/27/2020 02:59:38.464 AM onvifnvcPI Error http://172.19.232.75:80/onvif/subscribe_service: pull point socket exception.4/27/2020… Continue reading ONVIF Cameras May Stop Recording Motion