UniView NONE Branded IPC3618SB-ADF28KM-10 Motion works with 23.09

Description Motion events are not being received by exacqVision. Product Steps to Reproduce Expected Results Motion should work with 23.06 set up with Onvif Plugin. Actual Results Camera’s GUI shows motion events and we do not receive them. Solution Confirmed that 23.09 will allow the motion events to record and be seen in live view… Continue reading UniView NONE Branded IPC3618SB-ADF28KM-10 Motion works with 23.09

Avigilon H4A Multisensor Camera Not Connecting

Description  Avigilon H4A Multi-Sensor Camera s will not connect and are returning an OnvifnvcPI SOAP receive error. Product  Steps to Reproduce  Add an Avigilon H4A Multi-Sensor Camera Expected Results  Camera connects Actual Results  Camera fails to connect and returns the following log entriies SOAP Error 12/12/2022 02:48:38.640 PM (GMT-8:00) onvifnvcPI Error 172.41.100.124: soap receive error… Continue reading Avigilon H4A Multisensor Camera Not Connecting

Arecont cameras are not recording motion on server version 22.12

Description: Arecont cameras are not recording motion, and the motion tab is not showing on the cameras settings page The name of the camera is changing to AVCoster-Contera Resolution: The fix for the issue has been implemented on Version 22.12.115 you can download the Server from the links below Windows 64bit https://support.exacq.com/#/file-manager/file/51aeec4a-1fd0-46e1-8e54-05343684e274/exacq-vision-server-22-12-115-0-x64-exe Ubuntu 64bit https://support.exacq.com/#/file-manager/file/1e73f452-bd4e-484a-a52a-aa60a06def9a/exacq-vision-server-22-12-115-0-x64-deb… Continue reading Arecont cameras are not recording motion on server version 22.12

Are All ONVIF-conformant Cameras Compatible with ExacqVision Systems?

The streaming profile of ONVIF (Profile S) provides a standard interface for streaming video and audio between conformant devices (cameras or encoders) and clients (VMS). The ExacqVision VMS is listed as anĀ ONVIF Profile S-conformant client. Extensive testing with a wide variety of ONVIF Profile S-conformant cameras has revealed enough inconsistency that Exacq does not explicitly… Continue reading Are All ONVIF-conformant Cameras Compatible with ExacqVision Systems?

Pixelated Video on Bosch ONVIF Cameras

If live video from a Bosch ONVIF camera displays pixelization in exacqVision Client, complete the following steps: Browse to the camera’s advanced mode Encoder Profile page.Ensure that IP is selected in the GOP Structure drop-down list.Ensure that the I-frame Distance slider is configured for a low number (10, for example).Ensure that I-frame Quality and P-frame… Continue reading Pixelated Video on Bosch ONVIF Cameras