Description Cameras are not able to switch to Serial IP under Mechanical tab.Looking at the Onvif plugin the PTZ for the camera was set to “0”We could not enable it in the client. When attempting to set the serial to IP in the mechanical PTZ tab, it would flip back to the Serial Port to… Continue reading Allibi Camera ALI-PZ40-UZAI PTZ is disabled by default on 23.06-24.03
Tag: ONVIF Camera
Correcting Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif
Description Prior to the release of Cloudvue version 23.9 the error message “”Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif’” could appear when trying to add cameras to a Cloudvue Gateway. This will be fixed with the release of 23.9.x. Products Steps to Reproduce Add a new camera either by scanning or by IP. Expected Results Camera adds… Continue reading Correcting Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif
Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif
Description Prior to the release of Cloudvue version 23.9 the error message “”Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif’” could appear when trying to add cameras to a Cloudvue Gateway. This will be fixed with the release of 23.9. Products Steps to Reproduce Add a new camera either by scanning or by IP. Expected Results Camera adds… Continue reading Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif