We may have systems where people attempt to field upgrade their servers with an I/O board. Note that this is supposed to be for in house upgrade only. However some do fall through the cracks.
This is actually an eDVR board without the graphics chips. Here is the sequence to get it to work:
Let them physically install the card into the pci slot.
Run eDVRSetup to install driver.
Reboot
Stop the Server service.
Run SysPrep to configure system to include new eDVR board (which only has I/O).
Run Control Center to verify that the new board is recognized.
Reinstall exacqVision server software.