Symptom Samsung SNB-3002 cameras allow you to define non-detection motion areas. This is the opposite of most Samsung cameras, which allow you to define detection areas. There is no indication in exacqVision Client that an SNB-3002 camera motion window defines non-detection areas. <br> Workaround When using exaqVision Client to configure a motion area for an… Continue reading Samsung SNB-3002 Camera Allows Only Motion Non-detection Areas