Moving an eDVR Board in a Linux System

The following steps should be followed when moving the eDVR boards: In the exacqVision Client, save the system settings and note the serial number associated with the eDVR boards in the tree order by clicking on the board icons in the Configuration tree.Shut down the system.Unscrew the boards from the existing mounting. Do not disconnect… Continue reading Moving an eDVR Board in a Linux System