Time synchronization is an often overlooked concept in computer networking. The Network Time Protocol, also just shortened to NTP, is a network protocol and standard that allows distributed computers to synchronize their time. Why is this important? Keeping proper time on computers, particularly when dealing with several computers communicating with each other, is important for… Continue reading Explaining NTP
Tag: NTP Server Address
Dahua/Illustra Essentials plugin failed to post NTP server address on the camera at startup.
Description Dahua plugin which also supports Illustra Essentials failed to set the NTP server on the camera during initial connection time. By default if there is no override ntp server, the plugin should push the address of the server as NTP on the camera. <br> Version Introduced r71495 (dev build 6.5.38.71503/RC build 6.6.0.71575) <br> Platform All… Continue reading Dahua/Illustra Essentials plugin failed to post NTP server address on the camera at startup.