Can I run a Silent Install of ExacqVision?

ExacqVision Server and Client EXE installers adhere to the normal NSIS installation options. /S runs the installer silently.for silent. Example: exacqVision_23.0.3.6_x64.exe /S /D changes the installation directory. While the default directory is recommended, you may use this option to override it to install in another directory.Example: exacqVision_23.0.3.6_x64.exe /S /D=C:\Program Files\MyCustomDirectory More information about NSIS options can… Continue reading Can I run a Silent Install of ExacqVision?