Although ACTi TCM and KCM camera models allow dual streaming in MJPEG, MPEG-4, and H.264 video formats, they do not support motion detection in MJPEG format. Thus, the MJPEG option is not available on the Camera Setup page for those models in exacqVision Client. <br>
Tag: Not Supported
What IP cameras are supported by ExacqVision?
IP Camera Integration Database ExacqVision supports thousands of cameras from a large number of manufacturers. The IP Camera Integrations database provides a complete list of test records for supported camera models. Search by brand, model, or firmware version, and filter by camera feature. The following video describes how to use the database to its full… Continue reading What IP cameras are supported by ExacqVision?