Symptom When Illustra cameras are factory defaulted they have a gateway value of 0.0.0.0 in the network settings. Ubuntu servers use a mechanism called “reverse path filtering” set <br> Affected platforms Illustra Pro, Flex and Essentials camerasUbuntu 10.04, 12.04, 14.04 <br> Workaround Edit the network security configuration file in /etc/sysctl.d/Change the value from Strict mode… Continue reading Factory defaulted Illustra cameras cannot be discovered by exacqVision running on Ubuntu