Failed to Refresh Raid Controller – Arcconf config Missing Controller

Description  If a you have a Avnet Server with no Raid Card then you might see this logs spamming every minute.3/12/2025 12:00:57.103 AM (GMT-4:00) SysMgmtPI Error Failed to refresh RAID controller – arcconf config missing controller 3/12/2025 12:01:57.313 AM (GMT-4:00) SysMgmtPI Error Failed to refresh RAID controller – arcconf config missing controller 3/12/2025 12:02:57.537 AM… Continue reading Failed to Refresh Raid Controller – Arcconf config Missing Controller

Non-RAID A-Series Systems with LSI HBA Should Have Adjacent Drive Placement

The new F2A, A-Series chassis models will have front-loading drive bays. The front-loading bays will resemble the Z-Series, but these drives are not hot-swappable. This new model is a 2U chassis with 2 rows of drive bays in 4 columns for a total of 8 drive bays.  Bay 1Bay 2Bay 3Bay 4Bay 5Bay 6Bay 7Bay 8… Continue reading Non-RAID A-Series Systems with LSI HBA Should Have Adjacent Drive Placement