Adding Non-Licensed IP Devices When Licenses Are Full

When enabling an IP Device and all licenses are being used for cameras on the ExaqVision Server instance, a user will see an ExacqVision Client message indicating an error; that there are not enough available licenses to add additional devices. This error message appears via pop-up message or Client Indicator, then does not allow the… Continue reading Adding Non-Licensed IP Devices When Licenses Are Full