Arecont cameras are not recording motion on server version 22.12

Description: Arecont cameras are not recording motion, and the motion tab is not showing on the cameras settings page The name of the camera is changing to AVCoster-Contera Resolution: The fix for the issue has been implemented on Version 22.12.115 you can download the Server from the links below Windows 64bit https://support.exacq.com/#/file-manager/file/51aeec4a-1fd0-46e1-8e54-05343684e274/exacq-vision-server-22-12-115-0-x64-exe Ubuntu 64bit https://support.exacq.com/#/file-manager/file/1e73f452-bd4e-484a-a52a-aa60a06def9a/exacq-vision-server-22-12-115-0-x64-deb… Continue reading Arecont cameras are not recording motion on server version 22.12

Infinova – Onvif not triggering motion

Description When the Infinova camera is added there is no motion shown in the client Product  Steps to Reproduce  Expected Results  Motion is triggered Actual Results  No Motion seen on Exacq Solution Add the following to the section to the onvif JSON file in the server configuration. <br> Note: If upgraded this will be removed… Continue reading Infinova – Onvif not triggering motion

GSD – Onvif Not Triggering Motion

*** INTERNAL USE *** Description exacqVision Server is not detecting motion from GSD cameras using the onvif plugin. Product  Steps to Reproduce  Expected Results  Actual Results  Solution WARNING – This is temporary and will not survive an upgrade of exacqVision Server Software Modify the “options” section for “manufacturer”: “GSD” in the onvifnvcpi.json Note: See AES-69… Continue reading GSD – Onvif Not Triggering Motion