ESM downgrade fails with newly added users

Description Downgrading ESM from 4.5.10 or newer down to 4.5.9 or earlier can cause the following error. Also the installer fails not able to communicate with database. ERROR [installer:74] Exception in run_backward_migrations: Traceback (most recent call last): File “”, line 40, in run_migration_command File “south_utils\run_migrations.py”, line 127, in run_backward_migrations File “south_utils\run_migrations.py”, line 45, in run_migration_command… Continue reading ESM downgrade fails with newly added users