In order to export to a network drive, you first have to Map it. To Map a Network drive go to File Explorer in Windows. 1. Open File Explorer from the taskbar or the Start menu, or press the Windows logo key + E. 2. Select This PC from the left pane. Then, on the Computer tab, select Map network drive. 3. In the Drive list, select a drive letter.… Continue reading Exporting Video to a Network Share
Tag: Network Share
Auto Export to a Network Share from Linux-based Exacq Server
To configure auto export from a Linux-based Exacq Server to a network share, complete the following steps: (Windows procedure here)<br><br> NOTE: For Linux-based systems, this procedure is available in exacqVision Server/Client version 6.6 and later.<br><br> To remove the network target, complete the following steps: <br>
Auto Export to Windows Network Share from Windows-based Exacq Server
On a Windows system, exacqVision Server runs as a service. This is desirable because the service starts recording video without user interaction when the system is started. However, this creates an issue with the management of credentials for access to network storage, as the exacqVision Server does not run from a normal user account that… Continue reading Auto Export to Windows Network Share from Windows-based Exacq Server