Description Some Exacq NVRs built with Microsoft Windows Server 2022 only acknowledge one network interface, rather than two, when being configured out-of-box. <br> Product Issue has been noted on BBE systems ASRock Industrial IMB-X1313 system boards, listed below. NOTE: Windows Server OS is an optional upgrade for many systems, so this will not apply to… Continue reading Windows Server 2022 Showing Only One Network Card
Tag: Network Config
Incorrect Network Configuration when Importing exacqVision S-Series Settings
Importing settings from exacqVision Client to an exacqVision S-Series system can cause an incorrect network configuration. This can occur in the following situations: Exporting settings from exacqVision Client with network adapter bonding configuration (which is the default on S-Series systems).Importing settings on a system with no bonding, or a system with a bond name that… Continue reading Incorrect Network Configuration when Importing exacqVision S-Series Settings