Remote exacqVision Connection Diagrams

The method used for connecting to an exacqVision system from outside the LAN it resides on will depend on your network configuration and use case. Examples are provided below based on each method. Remote Connections Remote Connections are supported by exacqVision Server/Client 24.09 and above to facilitate connections from the exacqVision Mobile app. When considering… Continue reading Remote exacqVision Connection Diagrams

PortCheck Utility

When troubleshooting TCP/IP connectivity issues, it is often helpful to confirm that the network path is open over a specified port and that there is no interference from a firewall or antivirus. This also rules out software level problems that may be causing a failure to connect. While there exists many utilities to accomplish this… Continue reading PortCheck Utility

How multiple adapters on the same network are expected to behave

Summary If you configure a Windows-based computer that has more than one network adapter on the same physical network and protocol subnet, you may experience unexpected results. This article describes the expected behavior of this kind of nonstandard configuration.  More Information Consider the following scenario: In this scenario, you may expect the two adapters on… Continue reading How multiple adapters on the same network are expected to behave

Frequent Restarts on Linux Systems Archiving over Slow Network

Linux-based exacqVision servers could reboot frequently in certain conditions: Linux operating systemActive hardware monitoringArchiving over a slow network (WAN or other network with limited resources) This issue was fixed in version 6.3.33.65575, and it is available in public release 6.4. To work around this issue in affected versions, complete the following steps to configure an… Continue reading Frequent Restarts on Linux Systems Archiving over Slow Network

SCN-00000014 – ExacqVision Servers with Ubuntu 18.04 and Higher Network Troubleshooting

SCN #SCN-00000014Title of SCNExacqVision Servers with Ubuntu 18.04 and Higher Network TroubleshootingTRAC #Effective VersionApril, 2019Products AffectedServerReason for Change (Summary)Hardware manufacturing is now shipping all Linux systems (except the M-Series) with Ubuntu 18.04. Change Network troubleshooting in exacqVision Ubuntu systems has traditionally been accomplished using the ifupdown package of tools and commands.  ‘ifupdown’ is now deprecated… Continue reading SCN-00000014 – ExacqVision Servers with Ubuntu 18.04 and Higher Network Troubleshooting

Exacq Software/Service Connections Diagram

This diagram illustrates how the various Exacq applications work together and the ports used to communicate. Internal (LAN) Remote (WAN) In cases where external users plan to connect for remote monitoring, you will may need to configure port forwarding on your router to allow traffic on those ports to pass through. exacqVision provides several ways… Continue reading Exacq Software/Service Connections Diagram