Recording different resolution or frame rates on event

Description Some users may desire to record a different resolution or frame rate from a camera when an event such as motion or an analytic is triggered. Reasons for this vary by site, but often comes down to wishing to record a lower amount of data when very little is happening, but they require high… Continue reading Recording different resolution or frame rates on event

CSV Imports Exceeding IP Licenses

For the multi head camera when imported from a CSV file the client uses 4 camera licenses and not just one. This is true for all other manufactured multi head camera on the system in .CSV Previously we did not support this in our client. Dev build 21.09.2294700.0 included the following fix:Enhancement – Added support… Continue reading CSV Imports Exceeding IP Licenses