Description
With newer Samsung models that supports SUNAPI2. Only the first input trigger is activated for cameras that have multiple trigger inputs.
<br>
Version Introduced
- exacqVision Server 8.0.0.102418
<br>
Platform
All platforms for IP Cameras using Samsung plugin
<br>
Steps to reproduce
- Tested with SNP-L5233(00-09-18-41-34-F1 10.16.12.199) set with 4 input triggers
- Activate input triggers 2-4
<br>
Expected result
- Input triggers 1-4 correctly alarmed
- Event linking with each input trigger works as expected
<br>
Actual result
- Input triggers 2-4 are not alarmed
Work Around
- None
<br>
Version Fixed
exacqVision Server 8.1.4.102781
<br>