Description AV20576RS will show Motion recording in random recording states when updating Server to 24.12.7.0.In some Instances the cameras would allow some channels to recording while others stop seen below. Another issue seen was that motion would continuously record. Another Issue was observed where motion would just stop. Product Steps to Reproduce Update server to… Continue reading AVCostar AV20576RS Stop Recording Motion Properly When Updated to 24.12.7.0
Tag: Motion Issues
Illustra Pro Gen2 Domes 2/3/5 MP experiencing motion event issues
Description Affects 2/3/5MP Pro Gen2 Dome with motion set to ON and could not be turned off. This only affected Pro Gen2 DOME models.Models affected include:IPS02D2OCWITIPS02D2ISWITIPS03D2OCWITIPS03D3OCWITIPS03D2ISWITIPS05D2OCWIYIPS05D2ISWIY<br> Tested Version ExacqVision Server 8.0.4.104612 <br> Platform All platforms <br> Steps to reproduce Connect to a 2/3/5 megapixel Pro Gen2 Dome with firmware 1.2.0.Generate motion activity in the camera’s… Continue reading Illustra Pro Gen2 Domes 2/3/5 MP experiencing motion event issues