Wireshark Illustra Cameras for Motion Detection

NOTE: If you are experiencing trouble with motion recording using an Illustra camera on Exacq, please also refer to the following article, HERE. If you are attempting to confirm that motion detection is being sent from an Illustra camera to the VMS with Wireshark: 1. Be sure you are connecting to the camera via HTTP.… Continue reading Wireshark Illustra Cameras for Motion Detection

Axis plugin motion detection alarm event might not expire

Description Setting a Record Video via Video Motion Event will not clear on an Axis Q6114-E camera running Edge software. <br> Tested Version Edge 7.6.1.93449Firmware 6.20.1Client 7.6.4.94409 <br> Platform Edge <br> Steps to reproduce Set a Motion Window on the camera via the ClientConfirm Motion Detection is functionalCreate a new Event in Event Linking –… Continue reading Axis plugin motion detection alarm event might not expire