Motion and input trigger events stop working for Illustra cameras

Affected platforms exacqVision Server 5.10 or later with Illustra cameras using the Illustra3 plugin <br> Symptom When exacqVision reconnects to an Illustra camera during a stream restart, the socket connection communicating motion events and input trigger events could fail. If this happens, exacqVision will stop processing motion events and input trigger events.This is caused by… Continue reading Motion and input trigger events stop working for Illustra cameras