A-Series Desktop unit with Motherboard H110E1 is rebooting and stuck on the BIOS password page

Issue:- A-series Desktop unit is rebooting and stuck on the BIOS password page, And when checking in the BIOS, the system drive will be missing and needs to reboot to boot up to windows. Resolution:- There is an issue confirmed by the manufacturer that the new sound card that has been added to the A-Series… Continue reading A-Series Desktop unit with Motherboard H110E1 is rebooting and stuck on the BIOS password page

Updating Supermicro C7Q67 Motherboard Firmware

A small percentage of exacqVision systems with Supermicro C7Q67 motherboards installed have been found to exhibit widely fluctuating network performance and then lock up. The problem is known to occur only on systems containing Supermicro C7Q67 motherboards with theĀ BIOS firmware versionĀ 1.0b. These motherboards are found mostly in 2U exacqVision A Series and Z series servers.… Continue reading Updating Supermicro C7Q67 Motherboard Firmware