Description How to configure an ASRock system board if HDMI Output has been lost and both HDMI & VGA monitors are being used. Product Steps to Reproduce Expected Results Both monitors display video Actual Results Video is lost on both monitors Solution
Tag: Monitor
Configuring Multiple Monitors on Ubuntu Linux
Title exacqVision – Configuring Multiple Monitors on Ubuntu Linux Description If multiple monitors are attached you have the option to either mirror, show the same image on all monitors or extend the desktop. Configuration is done within the OS settings. Product Ubuntu LinuxexacqVision Solution Login to the OS as an adminLocate and select… Continue reading Configuring Multiple Monitors on Ubuntu Linux
System will not post without monitor attached
These files are only to be ran on ExacqVision Servers with the following Motherboards. DO NOT try to run it on your machine or it will cause issues!!! With the rise of new HIPPA requirements regarding patient information potentially being exposed on systems, a lot of customers are choosing to run their NVR’s Headless (no… Continue reading System will not post without monitor attached
Does the ExacqVision Client Support Multiple Monitors?
Yes, ExacqVision Client supports multiple monitors. We have tested up to four VGA monitors from a single workstation. Typically, a user will run one instance of the ExacqVision Client per monitor. Because decompressing video is CPU-intensive, we recommend one core per Client for the best user experience. To drive up to four VGA monitors, we… Continue reading Does the ExacqVision Client Support Multiple Monitors?