Affected platforms exacqVision 5.6.0 to 7.0 <br> Symptom When a new usbdio board is detected while the server is running, and it already has an input plugged in, the status of the input will not be updated in the client. <br> Workaround Restart the exacqVision server. This will result in a brief interruption of video… Continue reading The status of an input on USB module not updated if already connected when module plugged into server