Tag: MJPEG
Illustra Essentials low quality in MJPEG
Description When connecting to some essentials camaera’s OEM’ed by Dahua, the customer can put the camera in a mode that shows jpeg in a low quality and the quality slider has no apparent effect. To reproduce Workaround
MJPEG not supported on ACTi TCM and KCM cameras
Although ACTi TCM and KCM camera models allow dual streaming in MJPEG, MPEG-4, and H.264 video formats, they do not support motion detection in MJPEG format. Thus, the MJPEG option is not available on the Camera Setup page for those models in exacqVision Client. <br>