Some ExacqVision Client users report being unable to see the “Remote Connections” tab in some Environments. NOTE: This is typically an Operating System or Domain permissions issue. Products Steps to Reproduce In a restricted environment, or with a restricted user, launch the ExacqVision Client from the Desktop Icon, or folder. Expected Results When signed in… Continue reading Remote Connections node not visible in ExacqVision Client
Tag: Missing
Mechanical PTZ tab will not show up for Samsung cameras
When updating ExacqVision Server straight to 21.03 from a version prior to 9.8 the mechanical PTZ tab disappears. On the previous version below 9.8, update to ExacqVision Server 19.12 and verify the mechanical PTZ tab is there. Then update to ExacqVision Server 21.03 and verify the mechanical PTZ tab is there. If it is not,… Continue reading Mechanical PTZ tab will not show up for Samsung cameras