Configuring Multiple Monitors on Ubuntu Linux   

Title exacqVision – Configuring Multiple Monitors on Ubuntu Linux    Description  If multiple monitors are attached you have the option to either mirror, show the same image on all monitors or extend the desktop.  Configuration is done within the OS settings.   Product  Ubuntu LinuxexacqVision Solution Login to the OS as an adminLocate and select… Continue reading Configuring Multiple Monitors on Ubuntu Linux