This applies to both 14.04 and 16.04. We do not support 12.04 x64. <br> The steps are as follows: Back up your existing DVR configuration as a general precaution.Uninstall existing server and deps packages – apt-get remove edvrserver edvrserver-depsNote that this will properly preserve your existing DVR configuration, so that you should not have to additionally… Continue reading Migrating from 32-on-64 to 64-on-64 Linux
Tag: Migrating
Best Practice for Expanding an Array Using NTFS (Windows)
With hard drive offerings only increasing in size, it is important to remember that some large increases in RAID Arrays may not be read correctly by Windows. This is because there are limits to the cluster size that different sizes of volumes can use. If the volume is expanded beyond a cluster size limit, it… Continue reading Best Practice for Expanding an Array Using NTFS (Windows)