Missing Streams on Under Powered Multi-Sensor Cameras or Multi-View Devices

Description  Loss of video streams have been observed on multi-sensor cameras and multi-view devices because of the camera or device being under powered. Product  Expected Results  All video streams should connect and stream video Actual Results  3rd and 4th streams would occasionally disconnect and stop streaming Solution Follow the device manufacturer’s power recommendations and consider… Continue reading Missing Streams on Under Powered Multi-Sensor Cameras or Multi-View Devices

Connecting cameras over 100m in distance from G-Series PoE or Una recorders

ExacqVision G-Series PoE and Una recorders provide Power-over-Ethernet (PoE) ports for direct connections to cameras, rather than accessing cameras through a switched network. The TIA/EIA 568 standard provide that the maximum allowable length of a Cat5/5e or Cat6 cable is 100 meters (328 feet) for ethernet networks. To connect a camera farther than 100m away,… Continue reading Connecting cameras over 100m in distance from G-Series PoE or Una recorders