Description MegaRAID Storage Manager (MSM) has been found to have some exposure to CVE-2021-44228, the Apache Log4j remote code execution vulnerability, see statement from Broadcom Log4j2 Exposure (CVE-2021-44228). It is possible that MSM was installed on your exacqVision NVR even though a RAID controller card is not present. If that is the case MSM can… Continue reading Removing MegaRAID Storage Manager(MSM)
Tag: Microsoft Windows Operating System
Resizing a Partition on Microsoft Windows
Title Resizing a Partition on Microsoft Windows Description If the capacity of a virtual drive has been increased; once the reconstruction has successfully completed, then it will be necessary to resize existing partitions before the operating system can utilize the additional space. Product Microsoft WindowsexacqVision Server Overview Restart the NVRStop exacqVision Server ServiceLaunch Disk ManagementResize… Continue reading Resizing a Partition on Microsoft Windows
ExacqVision stance on updating the Windows Operating System
ExacqVision has tested and recommends the Windows 10 LTSB and LTSC releases from Microsoft. These are the only two releases we recommend and support.
Web Service upgraded from version 9.2 to 21.06+ on MS Windows operating systems fails to start
Issue: Upgrading the exacqVision Web Service from version 9.2 to version 21.06+ (even using the server bundled package) on Microsoft Windows operating systems will show the web service as upgraded but leave it unable to start. Root Cause: Undetermined. Workaround: After performing the upgrade, uninstall and reinstall the exacqVision Web Service again. Fixed Version: Not… Continue reading Web Service upgraded from version 9.2 to 21.06+ on MS Windows operating systems fails to start