Enterprise Manager memory resource usage high due to importer

Exacq Support has identified an issue with Enterprise Manager importer processes using an excessive amount of memory resource, often requiring reboot due to system becoming unresponsive when installed on some Windows machines. This is estimated to affect versions 23.06.2.0 thru latest versions of ExacqVision Enterprise Manager for Windows. Developers are aware and working on resolving… Continue reading Enterprise Manager memory resource usage high due to importer

Camera discovery plugin leaks memory

Affected platforms exacqVision 6.4 or higher <br> Symptom Every time there is a config or alarm event from core, the IP camera detect plugin (IPCamDetectPI.dll) will leak memory. The memory leak is in small increments and on systems where huge number of events are happening, like lots and lots of motion events for example, the… Continue reading Camera discovery plugin leaks memory