Dropping and Creating the smartvuedb Database

Description  At times it may be necessary to drop (delete) and create the smartvuedb database.  WARNING VIDEO LOSS is expected, and except for rare occasions this should only be performed on newly deployed NVRs. Product  Cloudvue Gateway Prerequisite Solution Issue the following commands from terminal ** WARNING ** WILL RESULT IN VIDEO LOSS <code>sudo service… Continue reading Dropping and Creating the smartvuedb Database

Cloudvue Gateway Camera Already Exists

Description  When attempting to add a camera to the Cloudvue Gateway an error message appears “Camera Already Exists”. Typically, this happens when the local database is out of sync with the cloud database. Removing the camera from the local database then re-adding triggers a new sync which resolve the issue. Below are instructions for removing… Continue reading Cloudvue Gateway Camera Already Exists