Categories
Knowledge Support Support Categories exacqVision Webservice Products

Manually Enabling Remote Web Service Configuration

THIS ARTICLE HAS BEEN DEPRECATED

By default, exacqVision Web Service restricts configuration to the browser on the local machine. Through the configuration, a user can disable this restriction to enable remote configuration. However, there could be a need to manually remove this restriction (such as when installing the Web Service in a virtual environment, such as exacqVision Virtual).

<br>

To manually enable remote configuration, complete the following steps:

<br>

NOTE: These instructions assume that the file to edit does not contain any text. If it has previously been changed, merge the changes specified here into the existing file.

  1. With administrator credentials, open the file .evws-login for editing. By default, this file is found in Windows at C:\Program Files (x86)\exacqVision\WebService\bin\.evws-login, or in Linux at /etc/.evws-login.
  2. Add the following into the file:

    [Settings]
    restricttolocalhost = 0
  3. Save the file.
  4. Restart the Web Service.

<br>

After restarting, the Web Service will have remote administration enabled.

<br>

You can also use the Web Service Configuration page to deselect the Enable Localhost Restriction option.