Tag: Manager
Enterprise Manager Groups
Increasing the Number of Connections Allowed in ESM
If an Enterprise System Manager (EM) installation is using the Postgres database with 500 or more servers, you could see the following error in the log file: “OperationalError: FATAL: sorry, too many clients already.”To increase the number of connections allowed, complete the following steps: <br> Stop all ESM services (ExacqVision Enterprise Manager Importer, ExacqVision Enterprise… Continue reading Increasing the Number of Connections Allowed in ESM