MAC OSX Clients Will Show a Cropped View of Cameras

Description  When using a single views either a multi camera view or a single camera view 2 different issues can be seen in a MAC client. 1. The image will be zoomed and will switch after 5-15 seconds back to a normal view- then back to a zoomed in Field of View.2. The image will… Continue reading MAC OSX Clients Will Show a Cropped View of Cameras

When exacqVision software is released, how long until the macOS and Linux versions are available?

All versions of exacqVision software are released at the same time because the code that runs on Windows is the same as the code that runs on the Linux and macOS platforms but compiled for each operating system. exacqVision Server, Web Service, and Enterprise Manager are currently available for Windows and Linux. The exacqVision Desktop… Continue reading When exacqVision software is released, how long until the macOS and Linux versions are available?