Description The following is a list of differences that will be found when comparing the exacqVision Client running on an M-Series server and that of the client running on any other machine. Product Embedded exacqVision ClientexacqVision M-Series Solution Important: These differences only apply to the exacqVision Client running on the M-Series itself! If you… Continue reading M-Series Embedded exacqVision Client Differences
Tag: M-Series
M-Series – Updating exacqVision Software
In order to comply with the NDAA “National Defense Authorization Act”, a two-step process is required to update an M-Series. First you must upgrade to version 20.03, then the server and webserver can be upgrade to the latest version. exacqVision Client versions higher than 20.03 are not supported. Note: The exacqVision Client version should not be… Continue reading M-Series – Updating exacqVision Software
Uninstall of Server May Leave Files Behind on Linux / M-Series
A normal uninstall of the the exacqVision Server software may leave plugin binaries behind in the plugin-store directory. Ubuntu: /usr/local/exacq/server/plugin-store M-series: /opt/exacq/server/plugin-store Fixed in exacqVision Server version 9.6.
M-Series Factory Default Fails
Symptom: Factory default of M-series fails. <br> Problem: M-series units produced in Q2 of 2017 have factory default backup stored at /mnt/ubifs/backup1 instead of /mnt/ubifs/backup . <br> Solution: Change the name of the /mnt/ubifs/backup1 directory to /mnt/ubifs/backup This bug is fixed in release ECN 170526-01
M-Series May Display False Watchdog Indications
Symptom: Log displays entries similar to the example below: 03/17/2018 11:06:11 AM LogPI Warning Stopping Log Manager. 03/17/2018 11:07:06 AM LogPI Warning Starting Log Manager 9.2.1.128741. 03/17/2018 11:07:08 AM dynacolorpi Warning Watchdog expired <br> Problem: This message is a false positive and can be ignored. <br> Solution: Update exacqVision Server version to 9.4 or higher.
Service Status Command Fails on M-Series or Ubuntu 10.04
Symptom: Unable to check status of exacqVision Server. <br> Problem: Running the Terminal command, ‘sudo service edvrserver status’ fails. Introduced with exacqVision Server version 7.6. <br> Solution: Update to exacqVision Server version 9.6.4
M-Series Translations
1. Start LXTerminal. 2. Change to admin user. su admin 3. Change to the admin home directory. cd 4. Download and execute the m-series script from translations server. curl -fsSL https://translate.exacq.com/m-series.sh | sh 5. Progress messages will scroll as the script executes. The last will be about installing the m-series lang. <br> Enable Translations The process… Continue reading M-Series Translations
How to update the M-Series recorder
** IMPORTANT ** Before updating please review Knowledge Base Article #6655 “M-Series – Updating exacqVision Software” for important information. M-Series recorders currently can be updated using two methods. ** IMPORTANT ** Before updating please review Knowledge Base Article #6655 “M-Series – Updating exacqVision Software” for important information. <br> Related Articles <br>
Web Service notes for M-Series performance
The following settings are recommended for ensuring the best performance of the web service on the M-Series: Start License: Change the recording format of each camera to “JPEG”.Pro License: Add a secondary stream for each camera, setting the recording format of the secondary stream to “JPEG”. Note: It may be necessary to create a view… Continue reading Web Service notes for M-Series performance
How to use the Surf web-browser on M-Series recorders
The M-Series recorders from exacqVision come with a web browser called Surf. Surf is a very basic web browser that is well suited to the capabilities of the M-Series recorder. Surf doesn’t have any window controls (address bar, back-button, etc.), so common browser tasks are accomplished with shortcut keys. Surf can be launched using the… Continue reading How to use the Surf web-browser on M-Series recorders