Error Code 49: Invalid Credentials When Logging Into LSA (LSI Storage Authority)

Description  LSI Storage Authority (LSA) fully supports English OS only, other languages are supported but a change to the LSA.conf file is necessary before you can login to LSA. Product  MegaRAIDLSI Storage Authority (LSA) Steps to Reproduce  Launch LSA from the desktop Enter the administrators username and password Expected Results  Login is successful and the LSI… Continue reading Error Code 49: Invalid Credentials When Logging Into LSA (LSI Storage Authority)

exacqVision Default Ports

Description  The following is a list of default port numbers used by exacqVision software. NOTE: Many ports listed below may only used with certain configurations or by optional services and integrations. Products Port List PortDescription25Simple Mail Transfer Protocol (SMTP)80exacqVision Web Server/exacqVision Enterprise Manager (HTTP)How to change Web Service portsHow to change EM web ports389LDAP (Lightweight… Continue reading exacqVision Default Ports

MegaRAID Definitions and Drive States

Description  Common definitions and drive states used in relation to MegaRAID RAID Controllers. Product  Virtual Drive A virtual drive is a partition in a drive group that is made up of contiguous data segments on the drives. A virtual drive can consist of these components: Drive Group A drive group is a group of physical… Continue reading MegaRAID Definitions and Drive States

Expanding a MegaRAID Virtual Drives Capacity using LSA  – Empty Slots Available

Title Expanding a MegaRAID Virtual Drives Capacity using LSA  – Empty Slots Available Description  Expanding a virtual drive means increasing its capacity. Existing data on the virtual drive is not impacted by the expansion. Follow these instructions to add a physical drive and expand the virtual disk size using LSI Storage Authority.   Expanding a RAID volume… Continue reading Expanding a MegaRAID Virtual Drives Capacity using LSA  – Empty Slots Available

Import or Clear Foreign Configurations Using LSA (LSI Storage Authority)

Title Import or Clear Foreign Configurations Using LSA (LSI Storage Authority) Description  A foreign configuration is a RAID configuration that already exists on a replacement set of drives that you install in a computer system. Product  MegaRAID 93xx Series RAID ControllerLSI Storage Authority Importing or Clearing the Foreign Configurations A foreign configuration is a RAID… Continue reading Import or Clear Foreign Configurations Using LSA (LSI Storage Authority)

Managing Physical Drives using LSA (LSI Storage Authority)

Description  All physical drives connected to the MegaRAID controller can be managed using LSI Storage Authority. Product  Start and Stop Locating a Drive If the physical drives are in a disk enclosure, you can identify them by making their LEDs blink.Perform the following steps to identify the physical drives. Making a Drive Offline Perform the… Continue reading Managing Physical Drives using LSA (LSI Storage Authority)

Silencing a MegaRAID Alarm Using LSA (LSI Storage Authority)

Description  Follow these instructions to silence MegaRAID alarms using LSI Storage Authority (LSA).  Product  Silence the Alarm When the controller detects an issue an alarm will occur and a high pitched beep will be emitted.  This alarm can be silenced through the LSI Software Authority. 

Creating a MegaRAID Virtual Drive Using LSA (LSI Storage Authority)

Title Creating a MegaRAID Virtual Drive Using LSA (LSI Storage Authority) Description  Follow these instructions to create a new virtual drive using LSI Storage Authority (LSA).  Product  MegaRAIDLSI Storage Authority (LSA) Overview  Stop exacqVision Server service Check current drive group and virtual drive configuration Create a new drive groupCreate a hot spare (optional) Create a new virtual drive Initialize the… Continue reading Creating a MegaRAID Virtual Drive Using LSA (LSI Storage Authority)

Deleting a MegaRAID Virtual Drive Using LSA (LSI Storage Authority)

Title Deleting a MegaRAID Virtual Drive Using LSA (LSI Storage Authority) Description  Instructions for deleting a MegaRAID virtual drive using LSA (LSI Storage Authority) Product  LSI Storage Authority MegaRAID Prerequisite Caution:  The exacqVision Server service should be stopped before proceeding Windows  Press Windows Key+R, type services.msc in the run box then press enterLocate and Stop the… Continue reading Deleting a MegaRAID Virtual Drive Using LSA (LSI Storage Authority)

Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Linux

Title Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Linux Description MSM has been found to have some exposure to CVE-2021-44228, the Apache Log4j remote code execution vulnerability, see statement from Broadcom Log4j2 Exposure (CVE-2021-44228).   As a result you may be able to replace MSM with LSA on a Windows machine using… Continue reading Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Linux