Title How to Identify the MegaRAID Controller Model on an exacqVision Server Description For various reason you may need to determine the model number of the RAID Controller Card. Product exacqVision Server MegaRAID Solution From the exacqVision Client Navigate to Configuration > YOURSERVER > Storage > Hardware Tab The model should be… Continue reading How to Identify the MegaRAID Controller Model on an exacqVision Server
Tag: LSI RAID Controller
Configuring exacqVision S-Series Enterprise System with LSI RAID Controller with all JBOD Disks
exacqVision S-Series systems with LSI RAID controller running exacqVision Server 6.4.x display an empty Network tab on the Storage page if all disks are configured for JBOD. To fix this issue, complete the following steps: On the S-Series system, download the udev_gen.sh script (attached below).cd to the location where the script was downloaded and run sudo ./udev_gen.sh.… Continue reading Configuring exacqVision S-Series Enterprise System with LSI RAID Controller with all JBOD Disks