Description MegaRAID Storage Manager (MSM) has been found to have some exposure to CVE-2021-44228, the Apache Log4j remote code execution vulnerability, see statement from Broadcom Log4j2 Exposure (CVE-2021-44228). It is possible that MSM was installed on your exacqVision NVR even though a RAID controller card is not present. If that is the case MSM can… Continue reading Removing MegaRAID Storage Manager(MSM)
Tag: LSI MSM
MegaRAID Definitions and Drive States
Description Common definitions and drive states used in relation to MegaRAID RAID Controllers. Product Virtual Drive A virtual drive is a partition in a drive group that is made up of contiguous data segments on the drives. A virtual drive can consist of these components: Drive Group A drive group is a group of physical… Continue reading MegaRAID Definitions and Drive States
Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Linux
Title Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Linux Description MSM has been found to have some exposure to CVE-2021-44228, the Apache Log4j remote code execution vulnerability, see statement from Broadcom Log4j2 Exposure (CVE-2021-44228). As a result you may be able to replace MSM with LSA on a Windows machine using… Continue reading Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Linux
Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Windows
Title Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Windows Description MSM has been found to have some exposure to CVE-2021-44228, the Apache Log4j remote code execution vulnerability, see statement from Broadcom Log4j2 Exposure (CVE-2021-44228). As a result you may be able to replace MSM with LSA using the following instructions. Product … Continue reading Replacing MegaRAID Storage Manager (MSM) With LSI Storage Authority (LSA) – Windows
Removing Unused LSI MegaRAID Storage Management Software on Ubuntu Linux to Eliminate Open Port 3071 Vulnerability
Vulnerability scans may detect and indicate that port 3071 is Open/Listening because of the installed LSI MegaRAID Storage Management software (LSI MSM) on an Ubuntu Linux server that does not have hardware support for RAID configuration. IF IT IS NOT BEING USED, the software may be removed to eliminate this vulnerability.