LSI Recommendations on Drive Capacity

To make the most efficient use of drive capacity, it is advisable to use drives of the same capacity. This is because the capacity of each drive is limited to the capacity of the smallest drive in the unit. Fault Tolerance: RAID TypeDescriptionRAID 5This type of unit provides performance, fault tolerance, and high storage efficiency.… Continue reading LSI Recommendations on Drive Capacity

Removing Unused LSI MegaRAID Storage Management Software on Ubuntu Linux to Eliminate Open Port 3071 Vulnerability

Vulnerability scans may detect and indicate that port 3071 is Open/Listening because of the installed LSI MegaRAID Storage Management software (LSI MSM) on an Ubuntu Linux server that does not have hardware support for RAID configuration. IF IT IS NOT BEING USED, the software may be removed to eliminate this vulnerability.